MCUXpresso terminates the debug session after a period of time (1 to maybe 20 minutes)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso terminates the debug session after a period of time (1 to maybe 20 minutes)

1,577件の閲覧回数
GregT
Contributor III

Until the termination all seems to be working. I can pause and run and also read memory. After the terminate I can Relaunch and continue debugging. Not sure how to debug this issue. Any ideas? Is there a log for the USB device that would give some clues?

FYI, the Debug window has this.
<terminated>New_configuration [GDB PEMicro Interface Debugging]
<terminated, exit value: 0>pegdbserver_console
<terminated, exit value: 0>arm-none-eabi-gdb
<terminated, exit value: 0>Semihosting Console 

The file window has this.
Break at address "0x7f92" with no debug information available, or outside of program code.

More info from the Debugger Console window.

Program received signal SIGTRAP, Trace/breakpoint trap.
0x00007f92 in ?? ()
Remote connection closed
Exception ignored in: <gdb._GdbOutputFile object at 0x7f8d50102880>
Traceback (most recent call last):
File "/usr/local/mcuxpressoide-11.8.1_1197/ide/plugins/com.nxp.mcuxpresso.tools.linux_11.8.1.202308071233/tools/share/gdb/python/gdb/__init__.py", line 47, in flush
def flush(self):
KeyboardInterrupt:

0 件の賞賛
返信
3 返答(返信)

1,545件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi @GregT 

To resolve your issue, please let us know

- your chip part number

- To identify if the problem is caused by specific project, can you please test if you can reproduce your issue with NXP SDK demo code?

Thanks,

Jun Zhang

 

0 件の賞賛
返信

1,539件の閲覧回数
GregT
Contributor III
Chip used is LPC18S37.
Where can I get NXP SDK demo code for that chip?

Thank you,
Greg
0 件の賞賛
返信

1,507件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @GregT 

For LPC18s37, there is demo under LPCopen, download from:

https://www.nxp.com/design/software/software-library/lpcopen-software-development-platform-lpc18xx:L...   

 

BR

Alice

 

0 件の賞賛
返信