MCUXpresso IDE v10.2.1_795 cannot debug

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE v10.2.1_795 cannot debug

1,290 Views
kiryat8
Contributor III

With MCUXpresso IDE v10.2.1_795 and also the previous version after building a debug project, I try to debug the program but the IDE gives an error when clicking to add a debug configuration. I cannot even open the debug configuration to try to edit it. My projects was created with previous MCUXpresso IDE versions.

I get an error after I click to create the debug configuration.

debug.jpg

0 Kudos
Reply
1 Reply

1,159 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Hi David,

There are indications from your screenshot that you are using a workspace from an older version of MCUXpresso IDE. Please be sure to use a new workspace and then build the project before attempting a debug operation.


Yours,

MCUXpresso IDE Support

0 Kudos
Reply