Am I just supposed to reinstall every few days?
Close to giving up on NXP. Freescale had it's problems, but never like this.
Translated Report (Full Report Below)
-------------------------------------
Incident Identifier: 1DEAD202-0730-4C08-A232-6B743F9BA845
CrashReporter Key: 11688060-EDB4-D2CB-E4F3-5DABB797DCFD
Hardware Model: MacBookPro16,1
Process: mcuxpressoide [3196]
Path: /Applications/MCUXpressoIDE_11.6.1_8255/*/MCUXpressoIDE.app/Contents/MacOS/mcuxpressoide
Identifier: MCUXpressoIDE
Version: 11.6.1 (11.6.1.202210031511)
Code Type: X86-64 (Native)
Role: Default
Parent Process: launchd [1]
Coalition: MCUXpressoIDE [3211]
Date/Time: 2023-01-20 17:48:56.7864 -0500
Launch Time: 2023-01-20 17:48:56.7641 -0500
OS Version: macOS 12.6.2 (21G320)
Release Type: User
Report Version: 104
Exception Type: EXC_CRASH (SIGKILL (Code Signature Invalid))
Exception Codes: 0x0000000000000000, 0x0000000000000000
Exception Note: EXC_CORPSE_NOTIFY
Termination Reason: CODESIGNING 1
Triggered by Thread: 0
Thread 0 Crashed:
0 0x1c1a7ae0 _dyld_start + 0
1 ??? 0xdb7b000 ???
Thread 0 crashed with X86 Thread State (64-bit):
rax: 0x0000000000000000 rbx: 0x0000000000000000 rcx: 0x0000000000000000 rdx: 0x0000000000000000
rdi: 0x0000000000000000 rsi: 0x0000000000000000 rbp: 0x0000000000000000 rsp: 0x00007ff7b2388ba8
r8: 0x0000000000000000 r9: 0x0000000000000000 r10: 0x0000000000000000 r11: 0x0000000000000000
r12: 0x0000000000000000 r13: 0x0000000000000000 r14: 0x0000000000000000 r15: 0x0000000000000000
rip: 0x000000001c1a7ae0 rfl: 0x0000000000000200 cr2: 0x0000000000000000
Logical CPU: 0
Error Code: 0x00000000
Trap Number: 0
Binary Images:
0x1c1a3000 - 0x1c20efff (*) <b53641ea-6cd4-39c9-9b14-59c92cfd9584>
0xdb7b000 - 0xdb7efff ??? (*) <bf0baa93-fe7a-3039-ac22-e0007dc821f4> ???
Error Formulating Crash Report:
dyld_process_snapshot_get_shared_cache failed
EOF
-----------
Full Report
-----------
{"app_name":"mcuxpressoide","timestamp":"2023-01-20 17:48:57.00 -0500","app_version":"11.6.1","slice_uuid":"bf0baa93-fe7a-3039-ac22-e0007dc821f4","build_version":"11.6.1.202210031511","platform":0,"bundleID":"MCUXpressoIDE","share_with_app_devs":1,"is_first_party":0,"bug_type":"309","os_version":"macOS 12.6.2 (21G320)","incident_id":"1DEAD202-0730-4C08-A232-6B743F9BA845","name":"mcuxpressoide"}
{
"uptime" : 3900,
"procLaunch" : "2023-01-20 17:48:56.7641 -0500",
"procRole" : "Default",
"version" : 2,
"userID" : 501,
"deployVersion" : 210,
"modelCode" : "MacBookPro16,1",
"procStartAbsTime" : 3967036934227,
"coalitionID" : 3211,
"osVersion" : {
"train" : "macOS 12.6.2",
"build" : "21G320",
"releaseType" : "User"
},
"captureTime" : "2023-01-20 17:48:56.7864 -0500",
"incident" : "1DEAD202-0730-4C08-A232-6B743F9BA845",
"bug_type" : "309",
"pid" : 3196,
"procExitAbsTime" : 3967058654630,
"cpuType" : "X86-64",
"procName" : "mcuxpressoide",
"procPath" : "\/Applications\/MCUXpressoIDE_11.6.1_8255\/*\/MCUXpressoIDE.app\/Contents\/MacOS\/mcuxpressoide",
"bundleInfo" : {"CFBundleShortVersionString":"11.6.1","CFBundleVersion":"11.6.1.202210031511","CFBundleIdentifier":"MCUXpressoIDE"},
"storeInfo" : {"deviceIdentifierForVendor":"03D58180-3E80-5B49-AFCD-C559064A5824","thirdParty":true},
"parentProc" : "launchd",
"parentPid" : 1,
"coalitionName" : "MCUXpressoIDE",
"crashReporterKey" : "11688060-EDB4-D2CB-E4F3-5DABB797DCFD",
"bridgeVersion" : {"build":"20P2059","train":"7.1"},
"sip" : "enabled",
"isCorpse" : 1,
"exception" : {"codes":"0x0000000000000000, 0x0000000000000000","rawCodes":[0,0],"type":"EXC_CRASH","signal":"SIGKILL (Code Signature Invalid)"},
"termination" : {"namespace":"CODESIGNING","flags":66,"code":1},
"extMods" : {"caller":{"thread_create":0,"thread_set_state":0,"task_for_pid":0},"system":{"thread_create":0,"thread_set_state":0,"task_for_pid":0},"targeted":{"thread_create":0,"thread_set_state":0,"task_for_pid":0},"warnings":0},
"faultingThread" : 0,
"threads" : [{"triggered":true,"id":54722,"threadState":{"r13":{"value":0},"rax":{"value":0},"rflags":{"value":512},"cpu":{"value":0},"r14":{"value":0},"rsi":{"value":0},"r8":{"value":0},"cr2":{"value":0},"rdx":{"value":0},"r10":{"value":0},"r9":{"value":0},"r15":{"value":0},"rbx":{"value":0},"trap":{"value":0},"err":{"value":0},"r11":{"value":0},"rip":{"value":471497440,"matchesCrashFrame":1},"rbp":{"value":0},"rsp":{"value":140701823699880},"r12":{"value":0},"rcx":{"value":0},"flavor":"x86_THREAD_STATE","rdi":{"value":0}},"frames":[{"imageOffset":19168,"symbol":"_dyld_start","symbolLocation":0,"imageIndex":0},{"imageOffset":0,"imageIndex":1}]}],
"usedImages" : [
{
"source" : "P",
"arch" : "x86_64",
"base" : 471478272,
"size" : 442368,
"uuid" : "b53641ea-6cd4-39c9-9b14-59c92cfd9584",
"path" : "\u0004",
"name" : "\u0004"
},
{
"size" : 16384,
"arch" : "x86_64",
"source" : "P",
"base" : 230141952,
"uuid" : "bf0baa93-fe7a-3039-ac22-e0007dc821f4"
}
],
"vmSummary" : "ReadOnly portion of Libraries: Total=672K resident=0K(0%) swapped_out_or_unallocated=672K(100%)\nWritable regions: Total=8192K written=0K(0%) resident=0K(0%) swapped_out=0K(0%) unallocated=8192K(100%)\n\n VIRTUAL REGION \nREGION TYPE SIZE COUNT (non-coalesced) \n=========== ======= ======= \nSTACK GUARD 56.0M 1 \nStack 8192K 1 \nVM_ALLOCATE 8K 2 \n__DATA 32K 2 \n__DATA_CONST 80K 1 \n__LINKEDIT 236K 3 \n__TEXT 448K 2 \n=========== ======= ======= \nTOTAL 64.8M 12 \n",
"legacyInfo" : {
"threadTriggered" : {
}
},
"trialInfo" : {
"rollouts" : [
{
"rolloutId" : "60da5e84ab0ca017dace9abf",
"factorPackIds" : {
},
"deploymentId" : 240000008
},
{
"rolloutId" : "60f8ddccefea4203d95cbeef",
"factorPackIds" : {
},
"deploymentId" : 240000021
}
],
"experiments" : [
]
},
"reportNotes" : [
"dyld_process_snapshot_get_shared_cache failed"
]
}
Model: MacBookPro16,1, BootROM 1916.60.2.0.0 (iBridge: 20.16.2059.0.0,0), 8 processors, 8-Core Intel Core i9, 2.3 GHz, 32 GB, SMC
Graphics: Intel UHD Graphics 630, Intel UHD Graphics 630, Built-In
Graphics: AMD Radeon Pro 5500M, AMD Radeon Pro 5500M, PCIe, 4 GB
Display: Color LCD, 3072 x 1920 Retina, Main, MirrorOff, Online
Display: BenQ SW2700, 2560 x 1440 (QHD/WQHD - Wide Quad High Definition), MirrorOff, Online
Display: ASUS PB278, 2560 x 1440 (QHD/WQHD - Wide Quad High Definition), MirrorOff, Online
Memory Module: BANK 0/ChannelA-DIMM0, 16 GB, DDR4, 2667 MHz, SK Hynix, HMAA2GS6CMR8K-VK
Memory Module: BANK 2/ChannelB-DIMM0, 16 GB, DDR4, 2667 MHz, SK Hynix, HMAA2GS6CMR8K-VK
AirPort: spairport_wireless_card_type_wifi (0x14E4, 0x7BF), wl0: Jul 12 2021 18:02:56 version 9.30.464.0.32.5.76 FWID 01-c081cfed
Bluetooth: Version (null), 0 services, 0 devices, 0 incoming serial ports
Network Service: Thunderbolt Ethernet Slot 1, Ethernet, en10
Network Service: Wi-Fi, AirPort, en0
PCI Card: pci1b21,1142, USB eXtensible Host Controller, Thunderbolt@72,0,0
PCI Card: ethernet, Ethernet Controller, Thunderbolt@71,0,0
USB Device: USB30Bus
USB Device: 4-Port USB 2.0 Hub
USB Device: 4-Port USB 2.0 Hub
USB Device: DAPLink CMSIS-DAP
USB Device: YubiKey OTP+FIDO+CCID
USB Device: USB2.0 Hub
USB Device: USB2.0 Hub
USB Device: USB3.0 Hub
USB Device: USB3.0 Hub
USB Device: Elements 25A3
USB Device: Elements 25A3
USB Device: Ultra Slim MT
USB Device: 4-Port USB 3.0 Hub
USB Device: 4-Port USB 3.0 Hub
USB Device: USB31Bus
USB Device: Plantronics BT600
USB Device: 4-Port USB 2.0 Hub
USB Device: 4-Port USB 2.0 Hub
USB Device: USB Receiver
USB Device: EPSON Scanner
USB Device: T2Bus
USB Device: composite_device
USB Device: Touch Bar Backlight
USB Device: Touch Bar Display
USB Device: Apple Internal Keyboard / Trackpad
USB Device: Headset
USB Device: Ambient Light Sensor
USB Device: FaceTime HD Camera (Built-in)
USB Device: Apple T2 Controller
Thunderbolt Bus: MacBook Pro, Apple Inc., 63.5
Thunderbolt Device: TB3-MiniDock-HM, CalDigit, Inc., 3, 33.1
Thunderbolt Bus: MacBook Pro, Apple Inc., 63.5
Same problem here.
So you are thinking that this will fix it:
% sudo codesign --force --sign - /Applications/MCUXpressoIDE_11.6.1_8255/ide/MCUXpressoIDE.app
Has anyone tried this? (I reinstalled, but it looks like installing a plug in makes it happen, so perhaps you guys could try and reproduce this?)
Try to install the EGit plug in as this is the only on I have installed.
I have the lasted version of eclipse and I installed several plug in and it seems fine. OF course that is a later version on Eclipse 2022-12 (4.26.0)
Hi,
Just noticed you also responded on the same topic on https://community.nxp.com/t5/MCUXpresso-IDE/I-ran-the-IDE-a-few-times-now-Mac-says-the-app-can-t-be-...
We will continue to look into it.
Regards,
MCUXpresso IDE Support
Hi,
There is a similar thread here: https://community.nxp.com/t5/MCUXpresso-IDE/MCUXpressoIDE-Code-Signature-Invalid-exception-when-laun...
As already mentioned in that thread, we do not have a fix we can do now in MCUXpresso IDE side. All Eclipse-based products seem are affected by this.
Here 2 links for problem description and possible workaround:
[1] https://bugs.eclipse.org/bugs/show_bug.cgi?id=578883
[2] https://developer.apple.com/forums/thread/684509
Regards,
MCUXpresso IDE Support