Lpcopen without board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Lpcopen without board

1,265 Views
jimprince
Contributor I

For 2 weeks I have tried to setup McuXpresso for my project, without success.

First, I have never been able to run Board wizard. "not a eclipse project"

2nd, I have not been able to make a board SDK. 

3rd, I have never been able to create a report from the config tool, no print available either.

4th I have entered pin labels into the configure tool, but it does nothing with the information ?

I am using LPC54113, I have have a custom board designed. I use gpio, pint interrupts (all of them) and 6/8 flexcomm channels. There is no LPC54113 board. I am using all of the pins. demo boards do not let you do that. 

I have never been able to include LpcOpen in a project without a board. 

Many people have talked all around this, but I have never seen a response that addresses the inability to get "board" drivers in a custom board build. 

Why not have a LcpOpen SDK ?

Why not have a custom board tool ?

 

0 Kudos
Reply
1 Reply

1,238 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

HI jimprince,

We have MCUXpresso SDK and configuration tools for LPC54113.

https://mcuxpresso.nxp.com/en/select

MCUXpresso SDK includes peripheral demo project. and user can easy to include the peripheral drivers to user application.

With MCUXpresso configuration tool, User can config pins, clock and peripherals. The configuration tools are integrated in MCUXpresso IDE.

The standalone configuration tool is also ready to use.

https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools-/mcuxpresso-c...

They are convenient tool for LPC users to develope custom board.

Hope this helps,

Jun Zhang

 

0 Kudos
Reply