Link HID - no emulator found error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Link HID - no emulator found error

3,012 Views
rohankanitkar
Contributor I

Hi,

I am using Windows 7 64 bit and MCUXpresso IDE v10.1.0 [Build 589] [2017-11-14]

When I try to program my ic by using Link server GUI flash programmer it give me following error:

Connect to target LPC 1769:
No compatible probes available. They may be disabled, disconnected, not powered, already in use or not compatible with this target.


Kindly advice. I am stuck.

Thanks
Rohan

0 Kudos
Reply
4 Replies

2,786 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Please ensure that you have disconnected your board from your PC.

Now open "Devices and Printers" in the Control Panel.

Now reconnected your board to your PC. Please tell us exactly what you see appear in "Devices and Printers".

Regards,

MCUXpresso IDE Support

0 Kudos
Reply

2,786 Views
lpcxpresso_supp
NXP Employee
NXP Employee

And what debug probe do you have connected between your PC and the target MCU? The LinkServer GUI flash programmer requires you to have a LinkServer compatible debug probe (so a CMSIS-DAP based probe such as LPC-Link2, or an original LPC-Link) connected between your PC and your target MCU. If you don't have such a debug probe, then there is no way you will be able to get this work.

Regards,

MCUXpresso IDE Support

0 Kudos
Reply

2,786 Views
rohankanitkar
Contributor I

My main aim to download the program in the MCU rather than debug. Kindly advice.

0 Kudos
Reply

2,787 Views
rohankanitkar
Contributor I

Hi,

I have LPC xpresso 1769 with CM SIS-DAP REV-D board with a mini usb connector and a normal USB cable.

0 Kudos
Reply