LPC1347 PWM cycle length issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LPC1347 PWM cycle length issue

1,633件の閲覧回数
mateuszkiełbasa
Contributor III

Hi community!

I'd like to write aplication to control PWM with 50Hz frequency and 1ms duty cycle using 16 bit timer. This is my code.

#include "board.h"

#include "../../static/inc/ct.h"
#include <cr_section_macros.h>

#define PRESCALE_VAL 36000 /* f = 72MHz, output T = 0.5ms => output f = 2kHz, 72MHz / 2kHZ = 36000 */

#define TIMER LPC_TIMER16_0
#define SYSCTL LPC_SYSCTL
#define IOCON LPC_IOCON

#define PWM_GPIO_PORT 0 /* PWM output port */
#define PWM_GPIO_PIN 8 /* PWM output pin */
#define IOCON_FUNC_PWM IOCON_FUNC2

#define PWM_MATCH_CHANNEL 0
#define PWM_RESET_CHANNEL 3

   int main(void) {
   // Generic initialization
   SystemCoreClockUpdate();
   Board_Init();

   IOCON->PIO0[PWM_GPIO_PIN] = IOCON_FUNC_PWM;
   SYSCTL->SYSAHBCLKCTRL |= CT16B0_CLOCK_MASK;
   Timer_Reset(TIMER);
   TIMER->PR = PRESCALE_VAL - 1;
   TIMER->MR[PWM_MATCH_CHANNEL] = 38; // 38 * 0.5 = 19ms
   TIMER->MR[PWM_RESET_CHANNEL] = 40; // 40 * 0.5 = 20ms
   TIMER->MCR |= TIMER_RESET_ON_MATCH(PWM_RESET_CHANNEL);
   TIMER->EMR |= _BIT(PWM_MATCH_CHANNEL);
   TIMER->PWMC |= _BIT(PWM_MATCH_CHANNEL) | _BIT(PWM_RESET_CHANNEL);
   TIMER->TCR |= TIMER_ENABLE_MASK;

   while(1) {}
   return 0 ;
}

I'm using logic states analyzer connected to the pwm pin. As a result I see that high state takes exactly 1.5ms (?) and low state takes 19ms (that's ok). My question is why duty cycle takes 1.5ms instead of 1ms?

0 件の賞賛
返信
2 返答(返信)

1,506件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Mateusz Kie&#322;basa,

Thank you for your interest in NXP Semiconductor products and 
for the opportunity to serve you.
It seems a bit strange.
I was wondering if you can tell me the cycle time of the match reset, and you can try set 39 instead of 40 likes below code.
TIMER->MR[PWM_RESET_CHANNEL] = 39 ‍

Have a great day,
TIC

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 件の賞賛
返信

1,506件の閲覧回数
mateuszkiełbasa
Contributor III

Thanks for your answer!

I checked and your solution works! Could you tell me why must I subtract one from this register value? It's incomprehensible for me...

Have a great day!

0 件の賞賛
返信