Hi,
I am using the KW45B41Z-EVK with MCUXpresso IDE.
The following examples run successfully:
- lpuart_polling
- freertos_hello
- flexcan_loopback_transfer
- connectivity_test_bm
However, BLE examples such as:
- wireless_uart_bm
- beacon_bm
fail during startup and stop at an NBU/rpmsg-related assertion before BLE advertising starts.
I also tried using SDK 26.09, but I am having difficulties importing some example projects into MCUXpresso IDE.
My questions are:
1. Are there any required NBU firmware images that must be programmed before running BLE examples?
2. Is there any additional setup required for BLE examples on the KW45B41Z-EVK?
3. Are there any known issues with SDK 26.09 example import in MCUXpresso IDE?
Any guidance would be greatly appreciated.
Thank you.