Is It possible to write a File from controller to PC(Only through Command Line)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is It possible to write a File from controller to PC(Only through Command Line)

1,712 Views
tosinghchandan
Contributor I

Hi MCUXprsso Team, I want to write a file from the controller to PC when MCUXpresso IDE is running and debugger(JLink/Link2) is connected, It is working fine. when I tried to write through command line where NO Ide is alive it is not happening. Is there any way to write into a file from the controller if MCUXpresso is not alive. I have used All commands for flashing and Reset for MCUXpresso only.

best regards

Chandan

Tags (1)
0 Kudos
Reply
1 Reply

1,638 Views
lpcxpresso_supp
NXP Employee
NXP Employee

No. File I/O from your ARM target application is done by a debugger servicing semihost calls. Without the debugger, there is no service.

Thanks and regards,

MCUXpresso Support

0 Kudos
Reply