I was wondering if MCUExpresso IDE offers capabilities similar to other IDE's to calculate the Peak RAM usage during executing of code.
I have a situation where I am running a converted .tflite file, and would like to see how big arena needs to be allocated to fit the model. TFLM does not support this, and I am afraid that I am writing outside of the allowed memory as the allocator only seems to consider the input size.
Is there a feature which can tell the peak RAM usage during runtime?
Solved! Go to Solution.
You can track dynamic memory usage including peak usage at runtime with this:
https://mcuoneclipse.com/2023/04/15/added-heap-memory-tracking-to-freertos-v10-5-1-using-systemview/
And there the 'Image Info' view which can be used for static memory: https://mcuoneclipse.com/2020/01/05/mcuxpresso-ide-v11-1-0/
If you are using FreeRTOS (which I assume), then there you have the stack watermark available: https://mcuoneclipse.com/2018/05/21/understanding-freertos-task-stack-usage-and-kernel-awarness-info...
Last but not least, you can use the following to determine heap and stack usage:
https://mcuoneclipse.com/2023/02/19/avoiding-stack-overflows-application-monitoring-the-stack-usage/
I hope this helps,
Erich
You can track dynamic memory usage including peak usage at runtime with this:
https://mcuoneclipse.com/2023/04/15/added-heap-memory-tracking-to-freertos-v10-5-1-using-systemview/
And there the 'Image Info' view which can be used for static memory: https://mcuoneclipse.com/2020/01/05/mcuxpresso-ide-v11-1-0/
If you are using FreeRTOS (which I assume), then there you have the stack watermark available: https://mcuoneclipse.com/2018/05/21/understanding-freertos-task-stack-usage-and-kernel-awarness-info...
Last but not least, you can use the following to determine heap and stack usage:
https://mcuoneclipse.com/2023/02/19/avoiding-stack-overflows-application-monitoring-the-stack-usage/
I hope this helps,
Erich