I can't get the Project Explore Window up .

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I can't get the Project Explore Window up .

ソリューションへジャンプ
3,729件の閲覧回数
jmanning
Contributor I

I can't get the Project Explore Window up .... When I go Window | Show View | there is not option for Project Explorer, not even under the option Other.

 

0 件の賞賛
返信
1 解決策
3,707件の閲覧回数
jmanning
Contributor I

Opening a new workspace brought back the option for Window | Show View |  Project Explore

Thank you !!!!!!!!!!!!!!!!

 

P.S. the reset perspective did not work

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
3,719件の閲覧回数
ErichStyger
Specialist I

Could you provide more details, please?

For example: which IDE version are you using?

Screenshots of what you see?

ErichStyger_0-1656566500479.png

 

And did you install any special plugins, or is this just a fresh install?

 

3,708件の閲覧回数
jmanning
Contributor I

Opening a new workspace brought back the option for Window | Show View |  Project Explore

Thank you !!!!!!!!!!!!!!!!

 

P.S. the reset perspective did not work

0 件の賞賛
返信
3,725件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello,

How about Reset Perspective: 

 

Alice_Yang_0-1656559120326.png

If still can't work, close the IDE, open it with new workspace.

 

 BR

Alice

 

0 件の賞賛
返信