How to get SVW data for further processing

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to get SVW data for further processing

1,808件の閲覧回数
kaihesse
Contributor I

Hi folks,

Im using the eclipse plugin impulse (http://toem.de) to visualize my trace data (e.g. SystemView).

On the LPC Xpresso 5411x I want to read the SWV data and formẃard to impulse to get analyzed.

How to fetch SWV data from the board and out of the IDE?

I see the data in the standard svw views. IS ther some way to store ?

Impulse can read it from tcp, file, pipe,serial,...

 

Best Regards,

Kai

タグ(2)
0 件の賞賛
返信
1 返信

1,701件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

No, sorry. MCUXpresso IDE's built in SWO trace support only with LPC-Link2 (as built into the LPCXpresso54114 board) with our own CMSIS-DAP firmware. The trace data streamed over a dedicated USB endpoint under the control of a proprietary client. There is currently no user access to this data.

To do what you want, you would need to use a different (external) debug probe and software solution on the host to process/save the trace data.

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信