How to change IDE language from Chinese to English

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change IDE language from Chinese to English

13,962 Views
samchen_tw
Contributor III

Hi,

I use MCUXpresso IDE v10.2.0 [Build 759] [2018-05-15] , how to change  IDE language from Chinese to English ?

Thanks.

Labels (1)
7 Replies

12,154 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Note : The above language setting only applies to the integrated Config Tools. The main IDE is English only and cannot be reconfigured.

Regards,

MCUXpresso IDE Support

0 Kudos
Reply

12,154 Views
BlackNight
NXP Employee
NXP Employee

It is possible add additional languages to the Eclipse IDE using Babel language packs: Do you Speak Klingon? How to change the Eclipse IDE UI Language with Babel | MCU on Eclipse 

Erich

12,154 Views
lpcxpresso_supp
NXP Employee
NXP Employee

What host computer OS and language configuration are you using? The main IDE does not provide any language settings - menus, dialogs, message etc are only provided in English. Can you share a screenshot?

Regards,

MCUXpresso IDE Support

0 Kudos
Reply

12,154 Views
samchen_tw
Contributor III

1. Windows 10 Professional

2. Language is Traditional ChineseMCUXpressoIDE.png

Thanks.

0 Kudos
Reply

12,154 Views
petrstruzka
NXP Employee
NXP Employee

Hi Sam,

if you have Chinese Windows locale, please add following lines to the end of mcuxpressoide.ini (you can find it in your installation \ide folder - like c:\nxp\MCUXpressoIDE_10.2.0_759\ide\mcuxpressoide.ini )

-Duser.language=en

(btw. to set it explicitly to Chinese, use -Duser.language=zh - simplified Chinese)

Petr

12,153 Views
samchen_tw
Contributor III

Hi Petr

It works.

Thanks you.

0 Kudos
Reply

12,152 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Sam,

I think you choosed Chinese when you install .

Please uninstall it , then select English when reinstall .

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply