How does the MCUXpresso IDE add variables to watch in the debug mode run state?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How does the MCUXpresso IDE add variables to watch in the debug mode run state?

10,135 次查看
neil168
Contributor I

Dear Sir.

How does the MCUXpresso IDE add variables to watch in the debug mode run state??

※Not debug paused add watch

Do you have to use those conditions??

thanks

0 项奖励
回复
11 回复数

9,854 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Although, as Erich says, the standard Eclipse/CDT Expressions view does not support live variables, you can achieve this directly in the Global Variables view. As well as supporting the addition of Variables (using the "spectacles" icon), the Global Variables view also provides an "Add new expression" option (inside the view itself, rather than in the view's icons).

In the below screenshot (debugging the K64/Bubble example), I am displaying the global "g_xAngle" as a variable, and also have added it as an expression too :

pastedImage_1.png

Regards,

MCUXpresso IDE Support

0 项奖励
回复

9,854 次查看
neil168
Contributor I

thanks

0 项奖励
回复

9,854 次查看
BlackNight
NXP Employee
NXP Employee
0 项奖励
回复

9,854 次查看
neil168
Contributor I

Dear Erich Styger,

Thank you for your reply, "Global Variables" window I have tried this function. Because of this function, the IDE will crash for a while, so I would like to ask if I have used Add Watch Expression and then observe it in Expression.
※ Hope is in the debug mode run mode Add Watch Expression

0 项奖励
回复

9,854 次查看
BlackNight
NXP Employee
NXP Employee

The expressions view does not support the live variable function. You have to use the variables view for this. If you want to monitor an expression, you would have to calculate that expression in your code and store it in a global variable instead.

0 项奖励
回复

9,854 次查看
neil168
Contributor I

thanks!!

0 项奖励
回复

9,854 次查看
BlackNight
NXP Employee
NXP Employee

Which IDE version and what debug connection are you using? Note that there has been an identified issue with P&E/SEGGER using live variables in IDE 11.0.0 which causes some unintended side effects. The LinkServer connection is not affected by that.

0 项奖励
回复

9,854 次查看
neil168
Contributor I

Dear Erich Styger,

I am using MCUXpresso IDE v11.0.0_2516, then I am using the P&E driver on NXP EVB to burn/debug, I will try to see what you said CMSIS drive to do this, but currently I use MCUXpresso IDE v11.0.0_2516 through CMSIS Driver also has a very unstable situation, I plan to use lpc-link2 to try again.

Thanks a lot...

0 项奖励
回复

9,854 次查看
neil168
Contributor I

pemicro.png

0 项奖励
回复

9,844 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi neilyen

Yes, we can take use of "Global Variables"  window. see attached video of how it works.

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

9,844 次查看
neil168
Contributor I

Dear Zhang Jennie,

Thank you for your reply, "Global Variables" window I have tried this function. Because of this function, the IDE will crash for a while, so I would like to ask if I have used Add Watch Expression and then observe it in Expression.
※ Hope is in the debug mode run mode Add Watch Expression

0 项奖励
回复