Github Copilot Plugin on MCUXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Github Copilot Plugin on MCUXpresso IDE

2,412件の閲覧回数
ksdbo52
Contributor II

Hi everyone,

I have been using MCUXpresso IDE for some time on our microcontroller project and use if for debugging on the target, too.

Some time ago we started working with Github Copilot. However, the official plugin cannot be installed, supposingly because most current MCUXpresso IDE 2025-06 is running on 2023 core runtime of eclipse, which does not fullfil copilot requirement of eclipse version 2024-03 or newer.

Can you provide a workaround or tell if an update is planned?

If others are interested in plugin support, it might be nice if you give a thumbs up or anything

Thanks,

Julian

タグ(4)
0 件の賞賛
返信
6 返答(返信)

2,311件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @ksdbo52 ,

You may consider using MCUXpresso for VS Code, which supports AI extensions such as Copilot, Gemini, and others.
BR
Celeste
0 件の賞賛
返信

2,241件の閲覧回数
ksdbo52
Contributor II

Hi Celeste,

Thanks for the recommendation. I already tried VSCode with the nxp plugin. However, I could not make it run.

We load our pre built .axf with a sdk example debug config for the imxrt1176 in MCUXpresso IDE. What is the migration path to VSCode?

Thanks,

Julian

0 件の賞賛
返信

2,183件の閲覧回数
luis_maravilla
NXP Employee
NXP Employee

Hello Julian,

The migration path for importing a project from MCUXpresso IDE to Visual Studio code is described in the next documentation.

MCUXpresso IDE Project Converter — MCUXpresso for VS Code documentation

After importing the project to Visual studio you could use the Binary Utilities option with the right click to create a .bin and then follow the steps to Flash the selected target, here is the link for the documentation Flash — MCUXpresso for VS Code documentation

Let me know if that work for you and if you need something else,

Best Regards, Luis

0 件の賞賛
返信

2,374件の閲覧回数
luis_maravilla
NXP Employee
NXP Employee

Hello Julian,

Could you help us share, what microcontroller are you using? And what OS are you using?

Best Regards, Luis

0 件の賞賛
返信

2,351件の閲覧回数
ksdbo52
Contributor II

Hi Luis, thanks, I am on MIMXRT1176DVMAA (FreeRtos) on Windows 11 Pro 25H2. Best, Julian

0 件の賞賛
返信

2,248件の閲覧回数
luis_maravilla
NXP Employee
NXP Employee

As mentioned in other comment, a workaround is using the MCUXpresso for VScode with the AI extensions.

Additional information on this tool for installing, flashing and debug, refer to MCUXpresso for VS Code documentation

Best Regards, Luis

0 件の賞賛
返信