Generate and keep compiler intermediary files

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Generate and keep compiler intermediary files

1,740 次查看
richardcopeman
Contributor II

HI,

I would like to be able to keep the compiler intermediary files (*.i). However, when I check the (Project->Properties->C/C++ Build -> Settings ->Tool Settings->Preprocessor->Preprocess only (-E) ) box and try to re-build the project I get a failure when the linker is invoked:

Building target: frdmk64f_coverage.axf
Invoking: MCU Linker
arm-none-eabi-gcc -nostdlib -Xlinker -Map="frdmk64f_coverage.map" -Xlinker --gc-sections -Xlinker -print-memory-usage -Xlinker --sort-section=alignment -mcpu=cortex-m4 -mfpu=fpv4-sp-d16 -mfloat-abi=hard -mthumb -T frdmk64f_coverage_hello_world_Debug.ld -o "frdmk64f_coverage.axf" ./utilities/fsl_assert.o ./utilities/fsl_debug_console.o ./utilities/fsl_io.o ./utilities/fsl_log.o ./utilities/fsl_str.o ./startup/startup_mk64f12.o ./source/main.o ./drivers/fsl_clock.o ./drivers/fsl_common.o ./drivers/fsl_ftfx_cache.o ./drivers/fsl_ftfx_controller.o ./drivers/fsl_ftfx_flash.o ./drivers/fsl_ftfx_flexnvm.o ./drivers/fsl_gpio.o ./drivers/fsl_smc.o ./drivers/fsl_uart.o ./board/src/board.o ./board/src/clock_config.o ./board/peripherals.o ./board/pin_mux.o ./CMSIS/system_MK64F12.o
./utilities/fsl_assert.o: file not recognized: File format not recognized
collect2.exe: error: ld returned 1 exit status
make: *** [frdmk64f_coverage.axf] Error 1

If I uncheck the box, then everything builds as normal.

Even with the failure, no .i files are generated.

How do I configure MCUXpresso to generate and keep these files for me?

TIA,

Richard.

0 项奖励
回复
1 回复

1,644 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Richard,

Try adding the '-save-temps' compiler option as a miscellaneous option. The details are documented in the GNU compiler manuals.

Thanks and regards,

MCUXpresso Support