FreeRTOS on FRDM-KE06Z using MCUXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeRTOS on FRDM-KE06Z using MCUXpresso IDE

2,629件の閲覧回数
jeya
Contributor I

I'm trying to create a sample FreeRTOS project on FRDM-KE06Z dev board using MCUXpresso IDE and could't find any sample project even on the SDK_2.x_FRDM-KE0z. Did imported SDK with CMSIS DSP Library, littlefs, FatFS, sdmmc stack, Amazon-FreeRTOS Kernel. Any help Thanks.

ラベル(1)
0 件の賞賛
返信
1 返信

2,453件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Jeya Sandi,

example project are provided for a board, so they are located in boards subfolder.

In MCU IDE, once SDK installed, go to Quickstart panel and select 'Import SDK example(s)' and follow the wizard.

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信