Failed to execute MI command: -target-select remote localhost:2331 on macos Sonoma 14.16.1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Failed to execute MI command: -target-select remote localhost:2331 on macos Sonoma 14.16.1

2,443件の閲覧回数
AleZeg
Contributor I

Kind All,

I'm a student tying to debug the first led_on-wait-led_off test exercise with MCUXpressoIDE. I'm using the software on my MacBook Air 8Gb M2 Sonoma 14.16.1. My J-Link debugger setting as default: I'm using the device MK22FN512xxx12 with Target Interface SWD connected via Bus USB 3.1. All the other students in the course are using same code/default setup/on Windows without any error, unfortunately me and another guy using Mac, every time we try to debug the project, we receive the related output:

Error in final launch sequence:

 

Failed to execute MI command:

-target-select remote localhost:2331

 

Error message from debugger back end:

localhost:2331: Operation timed out.

Failed to execute MI command:

-target-select remote localhost:2331

 

Error message from debugger back end:

localhost:2331: Operation timed out.

localhost:2331: Operation timed out.

 

Any help is greatly appreciated, thanks a lot!

0 件の賞賛
返信
1 返信

2,388件の閲覧回数
AdrianOltean
NXP Employee
NXP Employee

Please see the "Important note" here: MCUXpresso IDE v11.10.0 Now Available - NXP Community

AdrianOltean_0-1727073689966.pngAdrianOltean_0-1727073689966.png

Regards,

Adrian

0 件の賞賛
返信