Debug SEGGER J-link probes Error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debug SEGGER J-link probes Error

2,983 Views
WolfAlpha2
Contributor II

I import a SDK example of MIMXRT1052xxxxB board and debug it with SEGGER J-link probes (v7.60b) but I receive an error below. Help me known what happening ?

WolfAlpha2_0-1646128835365.png

 

0 Kudos
Reply
3 Replies

2,963 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To be prudent, I was wondering if you can introduce your testing environment, such as board, PC's OS, etc.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,956 Views
WolfAlpha2
Contributor II

Hardware:

- MIMXRT1050-EVK Evaluation Board

- Segger J-Link pro

Sofware: Mcuxpresso IDE v11.5, Windows 10

The first, i import SDK example with evkbimxrt1050 board. Next, I creat new Launch Configruration as SEGGER J-link probes. I build example project is ok. Then i check J-link pro connection also ok. I click debug with Segger J-link probes but Project is not running and a message show in Console Tab:

Executed SetRestartOnClose=1

[MCUXpresso Semihosting Telnet console for 'Example_RT1052_Ledoutput_igpio_led_output JLink Debug' started on port 8006 @ 127.0.0.1]

SEGGER J-Link GDB Server V7.60b - Terminal output channel


[Closed Telnet Session]

Please help me !

0 Kudos
Reply

2,948 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply and clarification.
Before debugging, I'd like to suggest you to open the J-link Commander to connect the board to check whether can recognize the core of the RT1052, if not, the debugging error must be the hardware connection.
Please give it a try.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply