DLAN-GREENPHY module Usage

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DLAN-GREENPHY module Usage

3,228件の閲覧回数
ssonsso
Contributor I

Hello.

I want to import the GreenPHY module Project into MCUXpresso following this site.

https://github.com/devolo/dlan-greenphy-sdk 

I have a problem in debugging process. (README.md - Usage - Step3)

"3. Now you should be able to see the SDK's folders in the Project Explorer. Select the wanted project (FirmwareStandalone or FirmwareStandaloneTFTP) and click on the blue debug icon or use Debug 'FirmwareStandalone(TFTP)' [Debug] in the Quickstart Panel and click the Resume button to start."

I clicked on it, but it doesn't debug.

I can't find availabe compatible probes and LinkServer/

I have attached a photo of the errors.

Could you give me a guide to solve these problems?

Thank you

0 件の賞賛
返信
1 返信

3,180件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi ssonsso 

The error messages show that MCUXpresso IDE doesn't find target.

To identify if this is related with a specific project. Please go to IDE "New project" to create an empty C project. Test if the empty project can connect the board

ZhangJennie_0-1672748090976.png

ZhangJennie_1-1672748112435.png

 

Have a nice day,

Jun Zhang

 

 

0 件の賞賛
返信