Convert to C++ Project - Fails with Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Convert to C++ Project - Fails with Error

1,435 次查看
GanesanGuru
Contributor IV

Hi fellas ,

I've converted project into C/C++ like this and I checked MCU C++ Includes are completely empty as attached below img..

Screenshot from 2023-11-08 15-10-57.png

 

Whether we should add an C++ Includes? - as its empty ash shown below..

Screenshot from 2023-11-08 16-32-27.png

 

Yet the C Include files remain intact - as shown below...

Screenshot from 2023-11-08 16-32-40.png

@frank_meyer ,  @davenadler can anyone helpme out form this issue!? It would be great if so!!!

标记 (2)
0 项奖励
回复
1 回复

1,404 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

HI GanesanGuru 

There are erpc related SDK demo code which includes C++. for example lpcxpresso55s69_erpc_matrix_multiply_rpmsg_cm33_core0

I think you can refer these C++ demo to configure your C++ project.

Have a nice day,

Jun Zhang

0 项奖励
回复