Can a program on the LPCEXpresso54608 be downloaded and debugged without Link2?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can a program on the LPCEXpresso54608 be downloaded and debugged without Link2?

2,187 次查看
tomstokland
Contributor I

The question says it all

4 回复数

2,068 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Just to follow up on Jennie's post. There is a debug interface built into the LPCXpresso54608 board that is functionally an LPC-Link2. Alternatively an external debug probe can also be used if required.

Yours,

MCUXpresso Support

0 项奖励
回复

2,068 次查看
tomstokland
Contributor I

The board doesn't show up either as a VSP or any other way. At this point I'm assuming it's defective.

0 项奖励
回复

2,068 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Maybe you can follow this  link to update the on-board firmware to see if this can fix the problem, in case the problem is not on the board defective.

https://community.nxp.com/message/925864 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

2,068 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

LPCXpresso 54008 on board debug probe supports CMSIS-DAP/SEGGER J-Link interface.

There is no option to simulate program without a board under MCUXpresso IDE.

Have a great day,
Jennie Zhang

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------