Build Server - Mcuxpressoidec: Java was started but returned exit code=1

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Build Server - Mcuxpressoidec: Java was started but returned exit code=1

ソリューションへジャンプ
6,377件の閲覧回数
elijah
Contributor III

I am setting up a build server for an MCUXpresso Project, and I have configured it to build the Release configuration. The build finishes correctly but the build server is reporting that it failed with the following message:

 

 

Mcuxpressoidec:
Java was started but returned exit code=1
-Djava.class.path=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\\plugins/org.eclipse.equinox.launcher_1.5.600.v20191014-2022.jar
-os win32
-ws win32
-arch x86_64
-launcher C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\mcuxpressoidec.exe
-name Mcuxpressoidec
--launcher.library C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\\plugins/org.eclipse.equinox.launcher.win32.win32.x86_64_1.1.1100.v20190907-0426\eclipse_1902.dll
-startup C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\\plugins/org.eclipse.equinox.launcher_1.5.600.v20191014-2022.jar
--launcher.overrideVmargs
-application org.eclipse.cdt.managedbuilder.core.headlessbuild
-import ./ProjectName
-cleanBuild ProjectName/Release
-vm C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\jre\bin\server\jvm.dll
-vmargs
-Djava.class.path=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\\plugins/org.eclipse.equinox.launcher_1.5.600.v20191014-2022.jar 
##[error]Process completed with exit code 1.

 

 

I am using a batch file to run the build with the following contents:

 

 

rem Batch file that builds firmware for release

@echo off

rem path to build tools
SET TOOLCHAIN_PATH=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\tools\bin

rem path to command line executable for MCUXpresso
SET IDE=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\mcuxpressoidec.exe

ECHO Extending PATH if not already present
ECHO %PATH%|findstr /i /c:"%TOOLCHAIN_PATH:"=%">nul || set PATH=%PATH%;%TOOLCHAIN_PATH%

ECHO Launching MCUXpresso IDE
"%IDE%" -nosplash --launcher.suppressErrors -application org.eclipse.cdt.managedbuilder.core.headlessbuild -import "./ProjectName" -cleanBuild ProjectName/Release

 

 

Manually running the batch file reports build succeeded with no errors, but the server reports it failed due to the Java error in mcuxpressoidec.exe.

How can I fix this issue?

0 件の賞賛
返信
1 解決策
6,118件の閲覧回数
elijah
Contributor III

I did fix it, I think I had to specify a workspace in the arguments when launching mcuxpressoidec.exe using -data "C:\MCUXpressoIDE_11.2.0_4120\workspace". My batch file is now:

 

rem Batch file that builds firmware for release

@echo off

rem path to build tools
SET TOOLCHAIN_PATH=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\tools\bin

rem path to command line executable for MCUXpresso
SET IDE=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\mcuxpressoidec.exe

ECHO Extending PATH if not already present
ECHO %PATH%|findstr /i /c:"%TOOLCHAIN_PATH:"=%">nul || set PATH=%PATH%;%TOOLCHAIN_PATH%

ECHO Launching MCUXpresso IDE
"%IDE%" -nosplash --launcher.suppressErrors  -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "C:\MCUXpressoIDE_11.2.0_4120\workspace" -import "./ProjName" -cleanBuild ProjName/Release

 


Useful link with a batch file that I played spot the difference with:
https://mcuoneclipse.com/2017/08/03/building-eclipse-and-mcuxpresso-ide-projects-from-the-command-li...

 

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
6,142件の閲覧回数
Smatt
Contributor I

I am encountering the same error. The build process itself is successful and reports 0 errors. Also a functional image is generated. 

However, eclipse exits with return code 1, which leads to the build automation system to register the build as failed. 

Could you solve the issue?

0 件の賞賛
返信
6,111件の閲覧回数
elijah
Contributor III

I did fix it, I had to specify a workspace in the arguments when launching mcuxpressoidec.exe using -data "C:\MCUXpressoIDE_11.2.0_4120\workspace". My batch file is now:

rem Batch file that builds firmware for release

@echo off

rem path to build tools
SET TOOLCHAIN_PATH=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\tools\bin

rem path to command line executable for MCUXpresso
SET IDE=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\mcuxpressoidec.exe

ECHO Extending PATH if not already present
ECHO %PATH%|findstr /i /c:"%TOOLCHAIN_PATH:"=%">nul || set PATH=%PATH%;%TOOLCHAIN_PATH%

ECHO Launching MCUXpresso IDE
"%IDE%" -nosplash --launcher.suppressErrors  -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "C:\MCUXpressoIDE_11.2.0_4120\workspace" -import "./ProjectName" -cleanBuild ProjectName/Release

Useful link that has a batch file that I played spot the difference with to find the issue:

https://mcuoneclipse.com/2017/08/03/building-eclipse-and-mcuxpresso-ide-projects-from-the-command-li...

0 件の賞賛
返信
6,119件の閲覧回数
elijah
Contributor III

I did fix it, I think I had to specify a workspace in the arguments when launching mcuxpressoidec.exe using -data "C:\MCUXpressoIDE_11.2.0_4120\workspace". My batch file is now:

 

rem Batch file that builds firmware for release

@echo off

rem path to build tools
SET TOOLCHAIN_PATH=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\tools\bin

rem path to command line executable for MCUXpresso
SET IDE=C:\nxp\MCUXpressoIDE_11.2.0_4120\ide\mcuxpressoidec.exe

ECHO Extending PATH if not already present
ECHO %PATH%|findstr /i /c:"%TOOLCHAIN_PATH:"=%">nul || set PATH=%PATH%;%TOOLCHAIN_PATH%

ECHO Launching MCUXpresso IDE
"%IDE%" -nosplash --launcher.suppressErrors  -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data "C:\MCUXpressoIDE_11.2.0_4120\workspace" -import "./ProjName" -cleanBuild ProjName/Release

 


Useful link with a batch file that I played spot the difference with:
https://mcuoneclipse.com/2017/08/03/building-eclipse-and-mcuxpresso-ide-projects-from-the-command-li...

 

0 件の賞賛
返信
6,109件の閲覧回数
elijah
Contributor III

https://mcuoneclipse.com/2017/08/03/building-eclipse-and-mcuxpresso-ide-projects-from-the-command-li...

I spotted a difference between the example here and my batch file, which was specifying a workspace.

0 件の賞賛
返信
6,370件の閲覧回数
converse
Senior Contributor V

I would guess that there *is* an error being reported in the build - check the complete build log.

0 件の賞賛
返信
6,355件の閲覧回数
elijah
Contributor III

I've checked through the whole log, the only error is the one in my post which appears at the end after the build finishes

0 件の賞賛
返信