Hi,
I'm using MCUXpresso 10.3, importing the provided LPC1769 examples.
lpc_chip_175x_6x for instance has the following section at the bottom of its .cproject file :
<storageModule moduleId="com.crt.config">
<projectStorage><?xml version="1.0" encoding="UTF-8"?>
<TargetConfig>
<Properties property_0="" property_2="LPC175x_6x_512.cfx" property_3="NXP" property_4="LPC1769"
[....]
<link href="nxp_lpcxxxx_peripheral.xme" show="embed" type="simple"/>
</info>
</infoList>
</TargetConfig></projectStorage>
</storageModule>
Depending on the OS, the IDE will automatically add or remove those independently from the chosen line ending and/or git attributes.
This is really annoying when trying to properly track changes on the projects configuration.
I have this issue too, exactly as described, using MCUXpresso 11.7.1. Looking forward to a fix!
Hi Julien Delbergue
Thank you for contacting us.
.cproject file contains project settings, such as building tools to be used, various compiler options, and so on.
Can you please upload your demo project to let us check the problem directly?
Besides, please also mention how we can reproduce your issue with your code.
Thanks.
Best Regards,
Hi ZhangJennie,
It should be quite easy to reproduce, independently from any specific project.
Here a detailed example:
1) On a Windows system
- Open MCUXpresso 10.3 (new/clean workspace)
- "Import project from file system" in the Quickstart panel
- Select "lpcopen_2_10_lpcxpresso_nxp_lpcxpresso_1769.zip" from the provided LPCOpen examples
- Select "lpc_chip_175x_6x" from the available projects
- Close MCUXpresso, and commit the imported "lpc_chip_175x_6x" project folder to a git repository
2) On a Linux system
- Clone the project repository, observe the clean git status
- Open MCUXpresso 10.3 (new/clean workspace)
- "Import project from file system" in the Quickstart panel
- Select the directory (unpacked) of the freshly cloned project
- Once the import is successful, close MCUXpresso
- git diff will show you the unwished modification of the .cproject file
The result is the same if going from Linux to Windows.
Thanks for your support.
HI
I current don't have a linux computer to test it.
Is the problem ( automatically add or remove those 
 ) the same if not using GIT?
Jennie Zhang
Thanks. Can you please upload both versions(windows,linux) of the .cproject files?
Any progress on this issue? I'm on MCUXpresso IDE 11.8.
I'm having the same problem, 4 years later. When I, a Windows user, save my project, the HTML code " " is added to every newline in the <projectStorage> tag of the .cproject file.
When Linux/Mac users save, the "#&13;" is then removed. It makes for some messy commits.
Unfortunately, it can't be resolved by git because it's not really newlines, but the HTML code for newlines.