Bitdefender marks MCUXpresso IDE as a virus

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Bitdefender marks MCUXpresso IDE as a virus

3,105 次查看
aberger
Senior Contributor I

I am using MCUXpresso IDE v10.1 (and have also checked with v10.0) and Bitdefender Internet Security 2018 on a Windows 10 PC. As soon as I initiate a build, Bitdefender begins quarantining mcuxpressoide.exe (causing the program to exit), and proceeds to quarantine lots of associated files.

Has anyone else experienced this? 

Adding the "\nxp\mcuxpressoide_10.1.0_589" folder to the Bitdefender exclusions list does not solve the problem. I have to completely deactivate Bitdefender in order to build a project in MCUXpresso.

Bitdefender claims that these files contain the "Gen.Atc4.Detection" virus.

0 项奖励
回复
1 回复

2,447 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Virus scanning on systems we have here are not showing any such issues (though we aren't using Bitdefender). If your are still seeing problems, I suggest you try again to prevent the scan of the IDE (How to add antivirus exclusions (exceptions) in Bitdefender 2018 ) or report it to them to as a false positive (What to do when Bitdefender detects legitimate applications).

Regards,

MCUXpresso IDE Support

0 项奖励
回复