ADC Data Average Using Timer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC Data Average Using Timer

1,511件の閲覧回数
Govind89
Contributor II

i am using km34z256xxx7 and i am using mcuxpresso sdk . I want to use a timer and an ADC interrupt handler. In this, I want to read ADC data every 1 second using an interrupt-based approach. When the timer starts, it will trigger the ADC to read and store the data in a buffer. Once the timer reaches 1 second, it will stop, and I will calculate the average of the ADC data in the buffer. After completing the average calculation, the timer will restart, and the process will repeat.

 #mcuxpressoide #nxp

0 件の賞賛
返信
1 返信

1,480件の閲覧回数
Celeste_Liu
NXP Employee
NXP Employee

Hello @Govind89 ,

Thanks for your post. This question is the repeat post, I will answer you in your private case which have the same question. 

Any updated information, please reply me in that case. Thanks for your understanding.

Have a great day,

Celeste

0 件の賞賛
返信