"Stalled on bus" - meaning

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

"Stalled on bus" - meaning

1,819 Views
cescvaro
Contributor II

Hi,

I'm trying to debug a LPC4330 on a custom board - as asked here https://community.nxp.com/message/1258844?commentID=1258844#comment-1258844 - and what happens is that as soon as the code of Reset Handler is executed and main is called, debug connection is lost and a message "Stalled on bus" or something similar appear in the bottom left of the IDE.

The debug probe, a LPC-Link 2, do not rise any error or message but for sure connection is lost, but processor keeps working fine.

My question is: what this error means? Where can I get more info or clue?

Also, why do not rise a warning or pop up? I mean, you have to pay attention to the status bar to notice it, and it is only showed for a short time.

regards,

fv

Tags (2)
0 Kudos
Reply
5 Replies

1,713 Views
soledad
NXP Employee
NXP Employee

Hi,

Could you please add a screenshot of your issue?

Regards

Soledad

0 Kudos
Reply

1,713 Views
cescvaro
Contributor II

Hi Soledad,

yes, sorry for the delay but I had no time to work on this project.

stalled.png

So this message apperas on the bottom left corner of the IDE, usually when I run a debug session.

regards,

fv

0 Kudos
Reply

1,713 Views
converse
Senior Contributor V

IIRC this happens when the processor is asleep (typically WFI).

0 Kudos
Reply

1,713 Views
cescvaro
Contributor II

Hi

are you sure? in WFI I tought the message is "Sleeping".

This "Stalled on bus operation" happens usually when I try to debug on a MCU with a program on external flash, when the PC jumps on the EXT SPIFI.

0 Kudos
Reply

1,713 Views
cescvaro
Contributor II

So,

nobody knows about this message on MCUXpresso ? Maybe I posted in a wrong area ?

thx.

fv

0 Kudos
Reply