Stuck at ResetISR function

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Stuck at ResetISR function

2,383 Views
Nikolas_M
Contributor I

Hello all, 

I have yet to be able to upload to my MIMXRT685-AUD-EVK. 

I am trying to run any of the SDK examples, and every time I hit debug It throws me into the ResetISR function and I cannot step. If I try and set a breakpoint, it says "The debugger has set two breakpoints at the same address 0x[insert address]". In the debugger console it says "monitor exec SetRestartOnClose=1". 

Any help would be appreciated!

 

Tags (1)
0 Kudos
Reply
2 Replies

2,369 Views
jeremyzhou
NXP Employee
NXP Employee

Hi @Nikolas_M ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you refer to the post.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

1,725 Views
yudeshui
Contributor II

Hi @jeremyzhou ,

I encountered the same issue now. Could you please share the post again to help me ?

Thanks in advance.

0 Kudos
Reply