Simulating a FRDM-KL25Z board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Simulating a FRDM-KL25Z board

4,113 Views
ptcaos
Contributor III

Hello,

 

because of COVID-19, I need to run some tests for my FRDM-KL25Z, but I have not got my board, so I would like to know if I could simulate this board in CodeWarrior 10.7 or 11.1.

 

Thanks!

0 Kudos
Reply
3 Replies

4,015 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

Unfortunately, we do not have a tool that simulates the freedom boards. As Erich mentions uTasker may be a good option. There is also a post by Mark, regarding a tool that may help in this case.

Having fun with the FRDM-KL25Z 

Best Regards,

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply

4,015 Views
ErichStyger
Specialist I

You might have a look at µTasker Kinetis FRDM-KL25Z support 

I hope this helps,

Erich

4,015 Views
ptcaos
Contributor III
0 Kudos
Reply