SAI Module for MKL16Z32VFM4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SAI Module for MKL16Z32VFM4

2,532 Views
joséviníciusmel
Contributor II

Hi,

I am working with the MKL16Z32VFM4 and I will use the SAI module.

I downloaded the SDK for MKL16Z32xxx4 devices, but I notice that the SDK folder (SDK_2.2.0_MKL16Z32xxx4.zip\devices\MKL16Z4) don't containt any SAI driver. I notice too that in MKL26Z4 folder there is SAI driver.

It is possible use the SAI driver of MKL26Z4 devices in MKL16Z4 devices?

0 Kudos
Reply
3 Replies

2,398 Views
mrluzeiro
Contributor I

I am experiencing the same issue.

I am porting a project from Kinetis to MCUexpresso and found this is not fixed yet

0 Kudos
Reply

2,398 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi José Vinícius Melo,

Yes. You can use the SAI driver of MKL26Z4 devices in MKL16Z4 devices.
Sorry for the inconvenience.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

2,398 Views
joséviníciusmel
Contributor II

Thanks Robin!

0 Kudos
Reply