Program the MKE16Z64VLF4 ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Program the MKE16Z64VLF4 ?

3,986件の閲覧回数
m_giraldi
Contributor II
I did a project that uses MKE16Z64VLF4, I used MCUXpresso to make the / fimware code (I generated the .S19), now I need to put it in production to write the MKE16Z64VLF4 without using MCUXpresso (production is 500 piece / month) , I couldn't use USBDM to record/Programming .S19 because it doesn't support MKE16Z64VLF4, I want to use NXP LPC-Link 2 to Record/Programming MKE16Z64VLF4, I use LPC-Link 2 on MCUXpresso to record and debug and it works perfectly, but I can't leave the firmware open in production to use MCUXpresso to burn the MKE16Z64VLF4, I ask:
1) Which app to use? How to do this?
2) Is there any tutorial to do this?
I already researched a lot and still can't solve it.

Note: On windows devices LPC-Link 2 is configured as follows: "LPC-Link-II CMSIS-DAP"
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,760件の閲覧回数
SANKENYXIA
Contributor I

MKE16Z64VLF4 CAN replace MKE15Z64VLF4?

0 件の賞賛
返信

3,881件の閲覧回数
converse
Senior Contributor V

Look for "Command Line Flash Programming" in the MCUXpresso User Guide. It describes how to do it.

0 件の賞賛
返信

3,759件の閲覧回数
SANKENYXIA
Contributor I

MKE16Z64VLF4 CAN replace MKE15Z64VLF4?

0 件の賞賛
返信