Hi, I'm researching on card communication with PN7462 card reader.
The example I use is PN7462AU_ex_phExCcid.
I use SCRTester Tool software and send data from the computer to the card reader with the command: 00 84 00 00 08, then the card reader sends data to the card
The computer receiving the data returns: A5 1D E4 E6 B3 59 E0 9A 90 00.
This means that the tag received the command and returned the data.
When I print the information of the pbInputBuffer() function I get the same data as the command sent from the computer
However, I did not find the function to send data from the PN7462 reader to the card and the function to receive data from the card to the PN7462 reader. Can someone help me with this problem?
Thanks & Best Regards