Multiple & Repeated Icons on Toolbar of MCU Xpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Multiple & Repeated Icons on Toolbar of MCU Xpresso

3,135 次查看
athmesh_n
Contributor IV

Hi, I have Updated my MCUXpresso to latest version - MCUXpresso IDE v11.1.0 [Build 3209] [2019-12-12].

The issue with IDE is irritating multiple and repeated on icons on toolbar. 

pastedImage_1.png

Please do provide a fix for this. Even though it doesn't affect the performance. It is surely irritating.

标签 (1)
标记 (1)
8 回复数

2,985 次查看
converse
Senior Contributor V

How did you update? Did you install to the same location as a previous installation? If yo did, this could be the cause of the problem. You should install to a fresh new location, not on the top of another install.

2,985 次查看
athmesh_n
Contributor IV

Okay, i dont remember how i did. But what should be done now?

0 项奖励
回复

2,985 次查看
converse
Senior Contributor V

Delete it and reinstall.

2,984 次查看
athmesh_n
Contributor IV

Okay! Thanks! I'll do and reply.

0 项奖励
回复

2,984 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello  ATHMESH NANDAKUMAR,

If still have the issue, please try to delete .metadata folder under workspace:

pastedImage_1.png

Regards

Alice

2,987 次查看
athmesh_n
Contributor IV

Thank you!

0 项奖励
回复

2,987 次查看
myke_predko
Senior Contributor III

Delete with extreme prejudice - I suggest that you delete the folder and when you reinstall, put MCUXpresso in a folder with a different name.  

You never know what Windows keeps around; if you want something deleted, kill it with fire.  

myke

2,987 次查看
athmesh_n
Contributor IV

Thanks for pointing that out. I am currently working on a project. Only after it is completed, I'll do the uninstallation and deletion, avoiding the risk factor.

0 项奖励
回复