MCUXpresso Driver Install Failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Driver Install Failed

965 Views
isabelheg
Contributor I

I am having trouble installing the driver for the MCUXpresso software on a Windows 10 Pro operating system using a FRDM K66F. When I attempt to install the driver, I get the error that the microcontroller can not be found, as shown in the image below. I have used the board and MCUXpresso IDE on a Mac operating system since the driver is built in, and am able to communicate and run code without a problem. Any advice or ideas on how to debug would be helpful.

0 Kudos
Reply
1 Reply

854 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Maybe you should update your FRDM-K66F openSDA firmware. Some peoples also faced this question Before.

https://os.mbed.com/questions/7465/FRDM-K64-The-driver-could-not-be-install/

Please visit OpenSDA Serial and Debug Adapter | NXP . Get new firmware and download to board. This problem will be fixed.

Regards,

Jing

0 Kudos
Reply