What is ip in clock_ip_name

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is ip in clock_ip_name

1,722件の閲覧回数
josephg
Contributor II

One of the many ways I learn is by understanding the naming of terms.  I understand clock and name in the term clock_ip_name but I am having a difficult time finding the reason behind ip.  Can someone please enlighten me about ip as it relates to clock_ip_name?  

Thank you.

0 件の賞賛
返信
3 返答(返信)

1,631件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Joseph,

 

IP stands for Intellectual Property.

 

Have a great day,
Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,631件の閲覧回数
nickdolling
Contributor IV

Felipe García wrote:

IP stands for Intellectual Property.

Seriously? That makes no sense in this context.

Nick

0 件の賞賛
返信

1,631件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hi Nick,

 

clock_ip_name refers to the clock of the specific IP module.

 

I recommend you to check the following post from the ARM community.

What is IP anyway? - Processors blog - Processors - Arm Community 

 

Best regards,

Felipe

0 件の賞賛
返信