MCUXPresso debugging issues

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXPresso debugging issues

ソリューションへジャンプ
4,101件の閲覧回数
nxf53819
NXP Employee
NXP Employee

Hi,

 I have encountered some issues while debugging in MCUXPresso with the LPC Link 2.

The problems occurred on Windows 10 with the MCUXPresso versions 11.0.0 and 11.0.1.

This is the error I get: "Em(01). Cannot find MEM-AP selected by core index (check target power)"

The complete error log is below:

error.PNG

I have got the same result with different LPC Link 2 debuggers and different boards.

Sometimes a reset (Windows restart, disconnect board and LPC-Link2, importing the project again in a new workspace) helps but most of the time it does not. And even if it works, after 1 debugging process it is back to the same issue again.

BR,

Simon

0 件の賞賛
返信
1 解決策
3,923件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Dear Simon,

I will suggest to change the LPC-Link2 firmware from CMSIS-DAP to J-Link. After this use the J-Link console and try to connect to your MCU using this console. Check the commands bellow:

pastedImage_1.png

Best Regards,

Alexis Andalon

元の投稿で解決策を見る

4 返答(返信)
3,923件の閲覧回数
nxf53819
NXP Employee
NXP Employee

Hi,

The number on my MCU is: MKL28Z512VLL7 1N52N

Regards,

Simon

0 件の賞賛
返信
3,924件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Dear Simon,

I will suggest to change the LPC-Link2 firmware from CMSIS-DAP to J-Link. After this use the J-Link console and try to connect to your MCU using this console. Check the commands bellow:

pastedImage_1.png

Best Regards,

Alexis Andalon

3,923件の閲覧回数
nxf53819
NXP Employee
NXP Employee

Dear Alexis,

I have programed the J-Link firmware onto my LPC-Link 2 and now everything seems to work again.

Thank you very much.

Best Regards,

Simon

0 件の賞賛
返信
3,923件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Hi Simon,

Sorry for the inconvenience. One detail you left missing is the Kinetis MCU part number and revision.

Thanks and regards,

MCUXpresso Support

0 件の賞賛
返信