Log file creation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Log file creation

2,464件の閲覧回数
sachin_singh
Contributor II

Hi All, 

I am working on the PN7462AU Eval kit for contact-less card (CL) for security systems.

And I need to generate the log file in the system which is connected with it.

So, Is there any way for its development and achieve it for keeping the track of CL card coming(to detect which card arrived at which time and also to detect any error if occurs so we can check it from log in system).

Thanks & Regards

Sachin

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

2,372件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please accept my apologies, but it has not been implemented for that specific use case. As far as I know, it is only possible to make a log in the console during the debug session with: phUser_Log_AU8(). Thank you for your comprehension.

BR,

Ivan.

0 件の賞賛
返信

2,372件の閲覧回数
sachin_singh
Contributor II

Okay Ivan.

0 件の賞賛
返信