Log file creation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Log file creation

2,451 Views
sachin_singh
Contributor II

Hi All, 

I am working on the PN7462AU Eval kit for contact-less card (CL) for security systems.

And I need to generate the log file in the system which is connected with it.

So, Is there any way for its development and achieve it for keeping the track of CL card coming(to detect which card arrived at which time and also to detect any error if occurs so we can check it from log in system).

Thanks & Regards

Sachin

Labels (1)
0 Kudos
Reply
2 Replies

2,359 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please accept my apologies, but it has not been implemented for that specific use case. As far as I know, it is only possible to make a log in the console during the debug session with: phUser_Log_AU8(). Thank you for your comprehension.

BR,

Ivan.

0 Kudos
Reply

2,359 Views
sachin_singh
Contributor II

Okay Ivan.

0 Kudos
Reply