Hi,
I just got a brand new LPCXpresso824-MAX Board, plugged it in and, apart from the 5V LED, nothing, no sign of life. (I thought that maybe the blinky program was pre loaded, but maybe not)
Anyway that's not the problem, MCUXpresso will not connect (see screen shot).
There is no UART connection for the board in the Device manager either.
I did install the 11U35 driver then realised that I have Win10 and didn't need to, but had the problem before I installed that.
I have rebooted the IDE and the computer. Still nothing.