Keil Ulink ProD support

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Keil Ulink ProD support

3,335件の閲覧回数
stephanie_kwan
Contributor I

Is the Keil Ulink Pro D a supported debug probe for MCUXpresso?

0 件の賞賛
返信
2 返答(返信)

3,066件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Kwan,

MCUXpresso support Keil uLINK with CMSIS-DAP firmware. http://www2.keil.com/mdk5/ulink

For more information, please see MCUXpresso_IDE_User_Guide.pdf under your MCUXpresso IDE install folder. 4.3 LinkServer Debug Connections

pastedImage_2.png


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,066件の閲覧回数
nxp69453
NXP Employee
NXP Employee

Hello Jennie Zhang,

   I am not sure if the new ULinkPro purchased would have CMSIS-DAP FW or not, but it is not getting detected as one of the Debugger connected to PC with MCUXpresso V10.3.0. Searched in Keil Website "http://www2.keil.com/mdk5/ulink" but was unable to find how to update the Keil ULink Pro FW to CMSIS-DAP.

Can you please provide with more information on the same?

Thanks and Regards,

Kiran Kumar