KL46 not visible in MCUXpresso Debug interface

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KL46 not visible in MCUXpresso Debug interface

943 Views
hpotsirhcreual
Contributor I

Hello, 

i have a FRDM-KL46Z board and want to debug an application with MCUXpreso but the OpenSDA interface from the board is not visible in MCUXpresso. 

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

881 Views
BlackNight
NXP Employee
NXP Employee

James,

if you are using Windows 10, you might be affected that the host OS overwrites the debug firmware on the board.

see Recovering OpenSDA Boards with Windows 10 | MCU on Eclipse  and especially Bricking and Recovering OpenSDA Boards in Windows 8 and 10 | MCU on Eclipse 

I hope this helps,

Erich

0 Kudos
Reply