Import KW2xD connectivity software example to MCUXpresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Import KW2xD connectivity software example to MCUXpresso

1,336件の閲覧回数
yuatliu
Contributor I

Hi,

I wonder if anyone has been able to import the examples from Kinetis MKW2xD and MCR20A Connectivity Software to MCUXpresso and manage to build it? It seems in the example files, there are only IAR and KDS project files. At first I thought MCUXpresso would also support KDS project files seamlessly, however, it is not like what I expected. If I import the examples from file system and try to build, MCUXpresso will remind me there si nothing to build. As NXP doesn't provide Thread stack MCUXpresso SDK for KW24D512 board, could anyone tell me how to import the examples and make them work under MCUXpresso? Or I have to download KDS to use these old examples?

thanks!

ラベル(1)
0 件の賞賛
返信
1 返信

1,278件の閲覧回数
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi Liu,

Unfortunately, the stack, for the KW24D and MCR20A, is only supported by IAR and KDS IDE.

Sorry for any inconvenience that this causes you

Regards,

Mario

0 件の賞賛
返信