IDE Debug Mode: Non Stop not available

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IDE Debug Mode: Non Stop not available

3,799 Views
shiv_aishwarya
Contributor I

I am currently evaluating MKV46F256 Tower Board and when I am importing any SDK Examples or creating new project. I am not able to see Non Stop Mode for Debug. I have read on forum that gdb server is not compatible with gdb non stop. How can we resolve this?

pastedImage_8.png

0 Kudos
Reply
6 Replies

3,676 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Debug sessions via P&E debug probes only support the use of all-stop debug mode (and not non-stop, which is only available when using a LinkServer debug connection, typically CMSIS-DAP). But this does not stop you from being able to debug with a P&E probe. What issue do you actually think you have?

Regards,

MCUXpresso IDE Support

0 Kudos
Reply

3,676 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

Please check below picture to update your MCUXpresso IDE software.

pastedImage_1.png


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

3,676 Views
shiv_aishwarya
Contributor I

It looks like there are no updates

pastedImage_1.png

0 Kudos
Reply

3,676 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I don't meet your mentioned issue during test.

Please try to update your board OpenSDA firmware with latest P&E OpenSDA image.

You could download it from here.

Wish it helps.


Have a great day,
Mike

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

3,676 Views
shiv_aishwarya
Contributor I

It didnt work. I have PE Micro Multilink Universal also. Even with that same issue is happening.

0 Kudos
Reply

3,676 Views
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi

For I could not regenerate the same issue on site, I would recommend to update on board OpenSDA firmware with Segger J-Link firmware so far.

Please check If J-LINK works. Thanks.

Best regards

Mike

0 Kudos
Reply