Hello NXP, I downloaded the new MCUXpresso IDE. It looks like everything loaded OK. I can build a project but when I click on Debug 'lpcxpreso54608_demo_apps_ I get an error message - No compatible probes available. They may be disabled, disconnected, not powered, already in use or not compatible with this target. I've checked the board where the jumper is supposed to go and it's installed but I think the board might be damaged. i got a used one from the Avnet FAI conference. Could that be the issue? Do I need a new board?