Embedded Artists LPC-link2 can boot and execute from flash?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Embedded Artists LPC-link2 can boot and execute from flash?

1,857件の閲覧回数
hungvuthai
Contributor I

Dear Sir,

Can I load Labtool firmware.bin in to flash of the LPC-Link2 board? Because I want to boot from flash and execute it directly, but I don't want boot from labtool.exe by DFU!. Could you please tell me how to do?

I tried load firmware.bin to flash (at 0x14000000 addr), then I closed JP1 on board LPC-Link2, reconnected USB to PC, the Embedded Artists LPC-link2 was connected with labtool.exe (device is availabe on labtool.exe ) but it do'nt do just like when using the DFU to boot! why?

I look forward to hearing from you as soon as possible!

Rgrds

HungVT

Embedded Artists LPC-link2 can boot and execute from flash?

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,750件の閲覧回数
hungvuthai
Contributor I

Thanks for your reply!

I read some above documents but have no information that i need yet!

Rgrds

HungVT

0 件の賞賛
返信

1,750件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Information on labtool can be found on the Embedded Artists website : LabTool - Embedded Artists 

I'm not very familiar with labtool, but it is possible that you might be able to produce an image suitable for programming into flash by using the "image manager" program. For more details see the documentation provided with LPCScrypt : https://www.nxp.com/lpcscrypt

Regards,

MCUXpresso IDE Support

0 件の賞賛
返信