MCUXpresso 26.09 Has Arrived: Here's What's New
If your workflow includes MCUXpresso, this release is worth a closer look.
Here's a breakdown of what's new and why it matters.
EdgeFast Open
MCUXpresso SDK 26.09.00 migrates from the EdgeFast Bluetooth stack for i.MX RT and MCX devices connected to an NXP radio co-processor (e.g., IW6xx devices) to the EdgeFast Open Bluetooth stack. EdgeFast Open is an open-source Bluetooth host stack based on the stack from the Zephyr community. This migration will make Bluetooth-based applications smaller size (Flash and RAM) due to architecture changes versus the previously used EdgeFast Bluetooth stack. Given that EdgeFast Bluetooth adopted Zephyr Bluetooth stack API’s the migration from EdgeFast Bluetooth to EdgeFast Open is expected to be minimally disruptive. For uses who want to continue using the EdgeFast Bluetooth stack, this continues to be supported and maintained on the SDK 26.06.00-LTS release that was introduced in Q2.
Documentation
SDK release notes have been updated to improve the quality, and relevance of results when using the built-in search tools. Example product documentation has also been reworked to improve readability, and useability in the web-based interface.
Security updates
Migration to MBEDTLS 3.x has been complete for all middleware components that depend on security. MBEDLS 4.2 is starting to be introduced into MCUXpresso SDK, offering a gradual transition to the next MBEDTLS LTS release.
RTOS updates
Updated FreeRTOS kernel and libraries for improved reliability, security and ecosystem compatibility
New product introduction support
MCXE327, MCXN556S (123-WLCSP), MCXN947T, MCXC352/353, MCXA556/557 (WLCSP), i.MX RT2660 , i.MX 93 Cortex-A55, i.MX 8M Mini Cortex-A53, i.MX 95 Cortex-A55, FRDM-IMXRT1152, FRDM-MCXE32B, KW43-LOC, MCXW70-LOC.
Toolchain and IDE updates
- IAR Embedded Workbench for Arm updated to v9.70.2
- MCUXpresso toolchain components aligned with the 26.06.00 release
Learn more: SDK documentation and GitHub Release Notes
Over the past three months, the MCUXpresso for Visual Studio Code team has delivered a series of updates focused on productivity, usability, and next-generation development workflows.
Experimental Agentic AI Toolkit
The headline feature this quarter is experimental access to the Agentic AI Toolkit, enabling developers to interact with MCUXpresso through AI coding assistants such as GitHub Copilot. Developers can install repositories, create and build projects, program devices, perform debugging tasks, and execute MCUXpresso-specific workflows directly from AI chat sessions.
Energy Measurement with MCU-Link Pro
LinkServer 26.09 introduces Target Power and Energy Measurement support for MCU-Link Pro and NXP development boards with power measurement circuits, providing visibility into device power and energy consumption directly within the development workflow. It includes both command-line and standalone GUI usage of the features. This helps developers better understand and optimize energy usage on their target hardware, up to CI/CD integration, and automated testing.
Easier Project Management
July and August releases delivered numerous customer-requested improvements that simplify everyday development, including faster project imports, improved repository management, more reliable project conversion from MCUXpresso IDE, better build configuration handling, and enhanced archive support.
Better DSP and eIQ Example Support
Developers working with DSP and eIQ examples will benefit from improved build automation that eliminates unnecessary toolchain errors when using supplied binaries, reducing setup complexity and improving the out-of-box experience.
Experimental Secure Debug Authentication
An additional experimental feature, Secure Debug Authentication, adds support for authenticating with protected devices before establishing a debug session when required by the device security configuration.
Explore the latest updates in the Visual Studio Marketplace Changelog and discover how MCUXpresso for VS Code continues to make embedded development more productive, intelligent, and efficient.
Learn more: MCUXpresso VS Code Documentation and Extension Change Log
MCUXpresso Secure Provisioning Tool (SEC) 26.09 - Broad coverage, stronger security, one unified tool
MCX Family Support & Improvement
- Added support for MCX E32x, L14x and W70x
- Secure Installer erasure improvement for MCX A1xx/2xx/3xx and L14x, L25x
Other significant updates
- Added support for i.MX RT1150, i.MX RT1185/118C, KW43 and i.MX 943 processors
- Debug authentication integrated into VS Code
Six clicks to secure your IP
- Blog — Prototype to secure deployment in six clicks
- Video — Six steps to secure your IP with MCUXpresso
- Training — How to build a secure image with MCUXpresso Secure Provisioning Tool
Learn more: MCUXpresso Secure Provisioning Tool
SPSDK 3.11.0 - Build your own secure production workflow
New features include:
- Added IPED tool for external flash encryption (nxpimage)
- Added debug mailbox command for MCX C1xx devices (nxpdebugmbox)
New devices supported include i.MX RT1150/1152, MCX A557, MCX E32x, MCX W70 and KW43 families.
Learn more: SPSDK
Config Tools 26.09 – Faster setup, timely insights
MCU Tools
- Now support preliminary public releases of processor data
i.MX Updates
- DDR Tool extended with new boards and memories
- System Manager has updated validation engine
Learn more: MCUXpresso Config tools and Config tools for i.MX release notes
Real-Time Edge 3.5 Released in July
- Fast Boot: Enables boot of two Cortex-A cores in parallel and decreases boot time especially for use cases with RTOS on Cortex-A core.
- Consolidated Images: Leveraging Yocto Multiconfig to enable single system image covering multiple boards (from same family).
- Updated Base: Now rebased on Linux Kernel 6.18.20 / Yocto Wrynose.
GUI Guider v2.0.1 Released in August
- Figma-to-GUI Guider import
- New UI for GUI Guider
- Visual flowchart-style event system
- Added FRDM-MCXA577, FRDM-MXCA287 & FRDM-MXCA266
- LVGL v9.4 support across MCX, RW, i.MX RT and i.MX platforms
MCU on Eclipse
- MCXC162 focused on Low-Power and Motor Control
- Remote-System Architectures
- High-Value Peripheral Enablement