Update SDK for existing Configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Update SDK for existing Configuration

2,391件の閲覧回数
benjaminnoack
Contributor I

Is it possible to update the SDK for an existing configuration? I have a project which I have been working on for a while and which is under source control. It was created with an older version of the Config Tools (v3.0). I can import the .mex file into Config Tools v4 but it gives me errors when trying to configure peripherals. It says my drivers are of an older version. I would like to be able to simply update the SDK from within the config tools.

0 件の賞賛
返信
1 返信

2,180件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Bejamin,

I'd recommend to create new project with same SDK drivers, and then copy new drivers to existing project. I'm not aware of any better alternative.

You can also use Peripherals with older version of SDK drivers. I've tried and I have not found any issue.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 件の賞賛
返信