Update SDK for existing Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Update SDK for existing Configuration

2,398 Views
benjaminnoack
Contributor I

Is it possible to update the SDK for an existing configuration? I have a project which I have been working on for a while and which is under source control. It was created with an older version of the Config Tools (v3.0). I can import the .mex file into Config Tools v4 but it gives me errors when trying to configure peripherals. It says my drivers are of an older version. I would like to be able to simply update the SDK from within the config tools.

0 Kudos
Reply
1 Reply

2,187 Views
marek-trmac
NXP Employee
NXP Employee

Hi Bejamin,

I'd recommend to create new project with same SDK drivers, and then copy new drivers to existing project. I'm not aware of any better alternative.

You can also use Peripherals with older version of SDK drivers. I've tried and I have not found any issue.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply