USB configuration created by ConfigTools

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

USB configuration created by ConfigTools

3,986 次查看
danielkrol
Contributor III

Hello,
When creating a new project using ConfigTools for USB there is a problem with a missing resource and there is no way to add it:
Zrzut ekranu 2025-02-23 o 12.09.30.png

The problem appeared since SDK 24.12.00. MCUXpresso for macOS. Tested for LPC55s69, MCX A153 and MCX N947.

 

Regards,

Daniel

0 项奖励
回复
7 回复数

3,967 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @danielkrol 

Please add the USB device CDC driver in the following way: Navigate to "Manage SDK Components", then select "USB middleware" and choose "USB CDC". The steps are shown as follows:

1.jpg

 

22.jpg

BR

Alice

0 项奖励
回复

3,916 次查看
danielkrol
Contributor III
Perhaps this matters - the problem occurs in MCUXpresso on macOS (Apple Silicon).

BR
Daniel
0 项奖励
回复

3,895 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @danielkrol 

Thank you for your question.

I have confirmed with internal Configure tool team. " MCUXpresso Config Tools 24.12.00 does not support the latest USB SDK middleware driver present in MCUXpresso SDK 24.12.00. The SDK 24.12.00 contains USB driver version 2.11.0, however, the Peripherals tool supports only drivers up to version 2.10.0. This issue is going to be fixed in MCUXpresso Config Tools 25.03.00 which will be released in second half of the March." Sorry for the inconvenience for you. So now, you can use SDK2.16.0. 

 

BR

Alice

0 项奖励
回复

3,310 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @danielkrol 

I'd like to share an update on this issue. I got a method from the MCUXpresso Config tool team, as shown below.

"

Please update Config Tools inside MCUXpresso IDE 24.12 to Config Tools 25.03:

  1. In MCUXpresso IDE, go to Help > Install New Software > Manage and enable the MCUXpresso Config Tools Update Site

Alice_Yang_0-1747201583410.png

2. Click Apply and Close and go to Help > Check for Updates. A new version of Config Tools will be available for installation. Finish the update using the update wizard.

Alice_Yang_1-1747201583431.png

"

 

Thank you.

BR

Alice

 

 

0 项奖励
回复

3,891 次查看
danielkrol
Contributor III
Hello,

OK, thank you!

BR
Daniel
0 项奖励
回复

3,955 次查看
danielkrol
Contributor III

Hello,

I know about that - all drivers are added. Even projects created in older versions of SDK stopped working. 

If I restore SDK 2.16.000 - everything works OK.


Regards
Daniel

0 项奖励
回复

3,459 次查看
danielkrol
Contributor III

Hello,

the problem is still not fixed in SDK 25.03.00.  There is the same error!

Regards
Daniel

0 项奖励
回复