There will be SDK update for

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

There will be SDK update for

1,877 Views
danielalvarenga
Contributor I

There will be SDK update for  SDK_2.2.0 from MK20DX256xxx10 to higher version? 

A ask that, because a desire to uso config flexcan on config tool from MCUXpress 11 , but a receive this message:

"Issue: Unsupported version of the FLEXCAN Driver in the toolchain/IDE project. Required: 2.2.3, actual: 2.2.0. Project might not compile correctly.
Level: Warning
Type: Validation
Tool: Toolchain/IDE project
Origin: Peripherals
Target: Toolchain/IDE project: core0
Resource: platform.drivers.flexcan"

Or is there a way to replace the CAN files?

1 Reply

1,782 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi, danielalvarenga

Unfortunately, there are now news regarding the version update of the SDK  for the  MK20DX256xxx10.

As you noticed the  SDK v.2.2.0 is not fully supported  by Peripherals tool. However  the differences between the available SDK version (2.2.0) and the required (2.2.3) may not be significant and probably will not  cause impact on the Tool functionaly, thus you can keep using that version . but I have mention that the driver  it is not tested.

If you experience problems, or require further support , please let me know!

Best regards, Diego.