Pins presets in SDK_24.12.00_FRDM-MCXA153

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pins presets in SDK_24.12.00_FRDM-MCXA153

Jump to solution
2,215 Views
danielkrol
Contributor III

Hello,
in the latest SDK_24.12.00_FRDM-MCXA153,  Config Tools -> Pins there is now only one basic preset: BOARD_InitPins.
Previously there were separate ones for LED, Buttons etc. Is this a deliberate change or some BUG?

Regards
Daniel

Pins.jpg

0 Kudos
Reply
1 Solution
2,184 Views
Lukas_Heczko
NXP Employee
NXP Employee

Hi Daniel,

Seems that MCUXpresso SDK board project templates does not support functional groups you are looking for in case of FRDM-MCXA153. As a workaround, you may try to create new FRDM-MCXA153 configuration in standalone version of MCUXpresso Config Tools, you'll see the functional groups there. Once you create the configuration, you can copy the generated .MEX file to your MCUXpresso IDE project.

Regards,

Lukas

View solution in original post

0 Kudos
Reply
4 Replies
2,194 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @danielkrol 

This is just a change. We can add the Functional Group  as follows:

 

55555.jpg

 

BR

Alice

0 Kudos
Reply
2,191 Views
danielkrol
Contributor III
Hello,

Thank you for your answer - I know how to add a Functional Group. However, I asked if the LEDs, BUTTONs etc. groups were permanently removed, because I am updating the instructions for students at my University.

Regards
Daniel
0 Kudos
Reply
2,185 Views
Lukas_Heczko
NXP Employee
NXP Employee

Hi Daniel,

Seems that MCUXpresso SDK board project templates does not support functional groups you are looking for in case of FRDM-MCXA153. As a workaround, you may try to create new FRDM-MCXA153 configuration in standalone version of MCUXpresso Config Tools, you'll see the functional groups there. Once you create the configuration, you can copy the generated .MEX file to your MCUXpresso IDE project.

Regards,

Lukas

0 Kudos
Reply
2,181 Views
danielkrol
Contributor III

Hello,

OK, thanks for your answer.

 

Regards

Daniel

0 Kudos
Reply